This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Assembly Macro Help

Greetings,

It was my understanding that there was an instruction, mov32, that would allow you to move a 32-bit value into a register. However, when I try to use this instruction I get a compiler error. It seems that the compiler does not recognize the instruction. I therefore decided to write a macro that would move a 32-bit value into a register. The code that I have written is shown below, but I am having some trouble compiling. I would appreciate any help with this code snippet.

movw		.macro	rx, n1, n2
mov rx, #n1, lsl #16
orr rx, rx, #n2
.endm

Kind Regards,
Willis