I am using the LM4f232H5QD Eval Board. I do not manage to trigger ADC0, Sequence0 with the downcounting event of PWM Module 1, Generator 2.
If I redirect the same PWM event to an interrupt and use the software trigger for the same ADC sequence, everything works fine.
So the general setup of PWM and ADC should be Ok. It's just that I somehow do not manage to trigger the sequence directly.
See the code on: http://pastebin.com/8YaBpHVy