Other Parts Discussed in Thread: EK-LM3S2965, LM3S2965
I am attempting to configure a CAN . I want to making a code like the following: Into the loop, continue to send a CAN Message.
When my code run ,it reaches the CAN interrupt handler.
But, go to default: only, because I checked resister value. As a result 0x40040004 000000E5.
This represents the bit 0 error. I do not know why this result.
Please help me.Thank you
Code1
void CANHandler(void)
{
unsigned long ulStatus;
ulStatus = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
switch(ulStatus)
{
case 10:
{
g_ulFlags &= (~FLAG_BUTTON_PEND );
break;
}
default:
{
CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
return;
}
}
CANIntClear(CAN0_BASE, ulStatus);
}
Code2
void main(void)
{
unsigned char EVENT_BUTTON_PRESS,TARGET_BUTTON_UP;
SysCtlClockSet(SYSCTL_USE_OSC | SYSCTL_OSC_INT);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinConfigure(GPIO_PE4_CAN0RX);
GPIOPinConfigure(GPIO_PE5_CAN0TX);
GPIOPinTypeCAN(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5);
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
CANInit(CAN0_BASE);
CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 1000000);
CANEnable(CAN0_BASE);
CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR);
/* ================================================================== */
/* = config message object = */
/* ================================================================== */
g_MsgObjectButton.ulMsgID = 0x0;
g_MsgObjectButton.ulMsgIDMask = 0;
g_MsgObjectButton.ulFlags = MSG_OBJ_TX_INT_ENABLE;
g_MsgObjectButton.ulMsgLen = 2;
g_MsgObjectButton.pucMsgData = g_pucButtonMsg;
IntEnable(INT_CAN0);
while(1)
{
SendButtonMsg(EVENT_BUTTON_PRESS, TARGET_BUTTON_UP);
}
}
Code3
void SendButtonMsg(unsigned char ucEvent, unsigned char ucButton)
{
//
// Set the flag to indicate that a button status is being sent.
//
g_ulFlags |= FLAG_BUTTON_PEND;
//
// Send the button status.
//
g_MsgObjectButton.pucMsgData[0] = 0x1;
g_MsgObjectButton.pucMsgData[1] = 0x2;
CANMessageSet(CAN0_BASE, 10, &g_MsgObjectButton,
MSG_OBJ_TYPE_TX);
}