This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The pin's function of RM48 MCU




Hello ,

 

I have a question about the pin's function of RM48 MCU.

I know the GIOA and GIOB were called GIO in document. and
GIOA support external interrupt capability.

Most of rest pin can work as a GIO. Do they support
external interrupt capability? or which pin also support external interrupt
capability like GIOA in rest of pins.

What is difference between the GIOA/B and rest of pins
which work as GIO?

Connected to stick, Are there just 10 pins of GIOA
(0,1,2,5,6,7)and GIOB(0,1,2,3) in the RM48l950PGE ?

Thanks!

 

Dison