Hi
I have difficulty to use the LM4F232 with Stellaris ICDI. The IDE is KEIL uVision4. It has complained one of the following:
Load "C:\\TI\\EKLM4F232\\boards\\ek-lm4f232\\blinky\\rvmdk\\blinky.AXF"
Connecting: Mode=JTAG, Speed=1000000Hz
Connection failed!, error code=&d
Load "C:\\TI\\EKLM4F232\\boards\\ek-lm4f232\\blinky\\rvmdk\\blinky.AXF"
Connecting: Mode=SWD, Speed=1000000Hz
Connection failed!, error code=&d
Does that mean I have to use a JTAG cable to debug my code instead of Stellaris ICDI?
Here is the Debug tab:
Here is the Debug settings:
In the above figure, the mode has to two options: one is SWD and the other JTAG.
Thanks,
-Hailin