Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Hello,
I was trying to run the HalGoGen 3.0 example : example_freeRTOSBlinky using a RM48 HDK.
I've followed the screens on HalCoGen help. AJusted the Include and compiler settings on my IAR and I got the following error :
"Error[Li005]: no definition for "_get_CPSR" [referenced from C:\Hercules\IAR\HCG_FREERTOS_BLINKY\Debug\Obj\os_port.o] "
I've tried to do a workaround.
I've added this code to the os_portasm.asm
-----------------------
;Get CPSR register
public vPortYield _get_CPSR
_get_CPSR
mrs r1,cpsr
bx lr
---------------------------
I also created a os_portasm.h and added the function stub:
#ifndef __OS_PORTASM__
#define __OS_PORTASM__
unsigned int _get_CPSR(void);
#endif
and included it on the os_port.c
There is any thing I'm missing ? is there some HalCoGen config that I've uset/not used that is messing up with the code.
Thanks,
Cristiano
/** @example example_freeRTOSBlinky.c* This is an example which descibes the steps to create an example application which * toggles the High End Timer (HET) pin 17 (LED in USB & HDK) based on the FreeRTOS timer tick of one second.** @b Step @b 1:** Create a new project.** Navigate: -> File -> New -> Project** @image html example_createProject.jpg "Figure: Create a new Project"** @b Step @b 2:** Configure driver code generation: * - Enable GIO driver* - Disable others** Navigate: -> TMS570LS3137/RM48L950ZWT_FREERTOS -> Driver Enable** @image html example_freeRTOSBlinky_enableDrivers_TMS570LS3x-RMx.jpg "Figure: Driver Configuration"** @b Step @b 3:** Configure Cortex-R4F IRQ handling: * - Disable IRQ handling via VIC contoller*het* Navigate: -> TMS570LS3137/RM48L950ZWT_FREERTOS -> Cortex-R4F** @image html example_freeRTOSBlinky_cortexR4F.jpg "Figure: Cortex-R4F Configuration"** @b Step @b 4:** Configure Interrupt handling: * - Enable SVC* - Enter FreeRTOS SVC handler name 'vPortYieldProcessor'* - Select IRQ dispatcher mode* - Enter FreeRTOS IRQ handler name '_IsrStub'** Navigate: -> TMS570LS3137/RM48L950ZWT_FREERTOS -> Interrupts** @image html example_freeRTOSBlinky_interrupts.jpg "Figure: Interrupt Configuration"** @b Step @b 5:** Configure VIM RAM: * - Enter FreeRTOS Timer Tick handler name 'vPreemptiveTick' at offset 0x0000000C** Navigate: -> TMS570LS3137/RM48L950ZWT_FREERTOS -> VIM RAM** @image html example_freeRTOSBlinky_VimRam.jpg "Figure: VIM RAM Configuration"** @b Step @b 6:** Configure Vectored Interrupt Module Channels: * - Enable VIM Channel 2* - Map VIM Channel 2 to IRQ** Navigate: -> TMS570LS3137/RM48L950ZWT_FREERTOS -> VIM Channel 0-31** @image html example_freeRTOSBlinky_vimChannelView.jpg "Figure: VIM Channel Configuration"** @b Step @b 7:** Configure OS timer tick to 1 ms: * - Enter Tick Rate of 1000** Navigate: -> OS -> General** @image html example_freeRTOSBlinky_osGeneral.jpg "Figure: OS General Configuration"** @b Step @b 8:** Generate code** Navigate: -> File -> Generate Code** @image html example_freeRTOS_generateCode.jpg "Figure: Generate Code"** @b Step @b 9:** Copy source code below into your application.** The example file example_freeRTOSBlinky.c can also be found in the examples folder: ../HALCoGen/examples** @note HALCoGen generates an enpty main function in sys_main.c, * please make sure that you link in the right main function or copy the source into the user code sections of this file.**//* Include common header file - types, definitions and function declarations for all drivers */#include "sys_common.h"
/* Include system header file - types, definitions and function declarations for system driver */#include "system.h"
/* Include FreeRTOS scheduler files */#include "FreeRTOS.h"#include "os_task.h"
/* Include HET header file - types, definitions and function declarations for system driver */#include "het.h"#include "esm.h"
/* Define Task Handles */xTaskHandle xTask1Handle;
/* Task1 */void vTask1(void *pvParameters){ for(;;) { /* Taggle HET[1] with timer tick */ gioSetBit(hetPORT1, 17, gioGetBit(hetPORT1, 17) ^ 1); vTaskDelay(100); } }
/* ESM interrupt notification (Not used but must be provided) */void esmGroup1Notification(unsigned channel){}void esmGroup2Notification(unsigned channel){}
/* GIO interrupt notification (Not used but must be provided) */void gioNotification(int bit){ return;}
/* USER CODE END */
/** @fn void main(void)* @brief Application main function* @note This function is empty by default.** This function is called after startup.* The user can use this function to implement the application.*/
/* USER CODE BEGIN (2) *//* USER CODE END */
void main(void){/* USER CODE BEGIN (3) */ /* Set high end timer GIO port hetPort pin direction to all output */ gioSetDirection(hetPORT1, 0xFFFFFFFF);
/* Create Task 1 */ if (xTaskCreate(vTask1, (const signed char *)"Task1", configMINIMAL_STACK_SIZE, NULL, 1, &xTask1Handle) != pdTRUE) { /* Task could not be created */ while(1); }
/* Start Scheduler */ vTaskStartScheduler();
/* Run forever */ while(1);/* USER CODE END */}
/* USER CODE BEGIN (4) */
/* USER CODE END */