This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Blown fuse F1 on RM48 HDK

Hi folks,

I have an issue with the fuse F1 on my RM48 HDK. It seems to be blown.

Do I need a special fuse or can I use any 2A quick blow fuse?

Regards,

Gregor

  • Gregor,

    Your question has been forwarded to our board expert.

    We will be back to you with and answer shortly.

    Regards,

    Jean-Marc

  • Gregor,

    Here is the part number for the fuse:

    Manufacturer:

     

    LITTELFUSE INC (VA)

    Part Number:

     

    F1397CT-ND

    Description:

     

    FUSE 2A 32V FST 0603 LEADFREE

    Technical/Catalog Information 0467002.NR
    Vendor Littelfuse Inc (VA)
    Category Circuit Protection
    Current 2A
    Voltage - Rated 32VAC, 32VDC
    Package / Case 0603 (1608 Metric)
    Fuse Type Fast Acting
    Mounting Type Surface Mount
    Lead Free Status Lead Free
    RoHS Status RoHS Compliant
    Other Names 0467002 NR
    0467002NR
    F1397DKR ND
    F1397DKRND
    F1397DKR

    Regards,

    Jean-Marc