Hello! I have a customer that has a question on correctly terminating the A/D inputs on their LM4F110H5QR.
According to Table 22-23 on Page 1104 of the LM4F110H5QR data sheet, the total equivalent a/d input resistance is 2.5k Ohms:
With this is mind, they designed the A/D input nets to have a maximum voltage of 18.229 Volts. This input voltage is applied through a 11.31k Ohm resistor connected to each A/D input pin. Their thoughts were the 11.31k Ohm resistor would form a divider with the 2.5k Ohm input resistance (RADC) to yield a maximum of 3.3 Volts at the a/d input.
Is their approach in calculating the total A/D input resistance - to set a maximum A/D input voltage of 3.3V correct? If not, then can you please advise what the resistor values should be?
Thanks!
Mark A.