Other Parts Discussed in Thread: HALCOGEN
Hello,
I have some questions regarding the NHET modules of the TMS570.
My concern is the usage of NHET for safety applications. Since it is possible to change the NHET code during run-time by changing the NHET RAM directly in the main c-code. Which makes the NHET not really relevant for safety applications I guess?!?
1) When using NHET for safety applications are there any issues that have to be considered in order to prevent "violation of RAM access" from ""outside" e.g. Bit manipulation?
2) Are there any safety aspects of the NHET?
3) How can the NHET (RAM) be verified?
4) Is the NHET certified?
5 )What if I want to use for example NHET1 for QM part and NHET2 for ASIL part.How can I make sure that both NHETs won't interfere with each other?
6) Are there some guidelines how to write NHET programs so that such problems can not occur?
Thanks in advance!
Regards, Albert