Hi,
I'm trying to debug my TMS570 board but I have troubles to do it, I know If I create a project and copy the axf file into the project directory , I should be able to debug the axf file without having to build the project again.,
Now, I try to debug an axf file ( (it is called Blinky file demo on Keil) )however i have the following error:---- flash download failed
I'm using target debugging with J-Link and an R4 controller ,I am configure the options target in order to use J-Link ...
Please Somebody can help me?