Other Parts Discussed in Thread: HALCOGEN
Hi,
I got TMS570LS31x Hercules Development Kit, and want to use the external 8MB SDRAM.
But, it seems that I can't access SDRAM.
Is there any initialization step to use SDRAM?
I made TMDX570LS31HDK project by HALCoGen(2.09.001) and "Generate Code" default settings.
I added some callback funcs and build projects CCS(4.2.5.00005).
In main func, I added the following codes to check access to SDRAM.
volatile int *p = (volatile int*)0x80000010;
int tmp0, tmp1, tmp2;
void main(void)
{
tmp0 = *p;
*p = 1234;
tmp1 = *p;
*p = 5678;
tmp2 = *p;
}
I watched tmp0,tmp1,tmp2 by debugger, but these values '0' (sometimes'-1409474866').
I checked HALCoGen settings.
- Mpu setting Region 6 Configuration is
checked 'Enable Mpu Region'
Base Address : 0x80000000
Size : 128_MB
End Address : 0x87ffffff
no check Disable Sub-Region 0 to 7
Type : STRONGLYORDERD_SHAREABLE
Permission : PRIV_RW_USER_RW_EXEC
- No EMIF setting tab
What can I do to access SDRAM?
Please help me!