Other Parts Discussed in Thread: HALCOGEN
Hello
I am currently evaluating the RM48 USB MCU Development Kit and get an error when trying to flash the device.
I use nowFlash and get the following Error:
Error 199 - Unable to connect to target on port address 0x000.
I was able to connect to the target until I changed the Clock Soure in HalCoGen from PLL1 to LPO_High and flashed the new build to the USB Kit.
When I was using the PLL1 option, the device worked with a core frequency of 160 MHz.
Thanks in advance,
Fuchs Dominik