This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI strange behavior with CCS compilation

Hi,

I'm using CCS v5.1 with LM4F232H5QD with sysclk set to 1Mhz.

I'm compiling the same code with CCS and IAR and I see different SPI behavior with the CCS compiled version.

The issue arises during the first SPI transfer between the host and a specific module. The SPI transfer is with the help of DMA.

I notice two strange behaviors:

1. My first SPI write is 4 bytes, 50 ms pause and then write 6 byte. I can see on the scope the first 4 byes correctly, but then I can see only 4 bytes out of the 6. (clock was 1khz confirmed to the scope).

2. I divided the 6 bytes to 4 and then 2 bytes (meaning 4 bytes, then another 4 bytes and the 2 bytes left) and then the written was successful (?).  The next action is SPI read from the module. Suddenly I see that the clock dropped to 8KHz.. When I reviewed the registers I say that SSI_CPSR (the divider) was change from 0x2 to 0xFE. It was change exactly during activating MAP_SSIDMAEnable().

Is there any reason why I can’t transfer more than 4 bytes on the SPI?

Is there any reason why the divided is overwritten?

I just want to mention that the same code exactly works perfectly when compiling with IAR - none of these phenomenons happens.

Thanks for your help!

Yael