This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fast data exchange between two tms 570 mcu

Hello,

i need a fast data exchange between two tms 570 mcu. One mcu (master) should be read from and write to the other mcu (slave)  to desired ram areas for data exchange. I think a combination  with the DMM and RTP module are the right way? Is there some application notes to connect two tms 570 each other with the DMM / RTP interface to obtain a fast data interchange between both mcu described above.

Thanks in advance.