This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Memory Error in PBIST Self Test

I have added the PBIST test, but the callback function "memoryPort<X>TestFailNotification" are called 3 times,

2 for port 1 and 1 for port 2.

the values are the following :

groupSelect dataSelect address data
Port 0, 1st 0x4 0x20 0x0 0xFFFFFFFF
Port 0, 2nd 0x4 0x21 0x0 0xFFFFFFFF
Port 1 0x4 0x21 0x0 0x1

for what I can tell reading from the PBIST sequence in the Ref. Manual, 7.3.1,

I should get from the PBIST run

RGS and RDS values ( table 7.1 )

Failure Count

Memory Address Offset of the first failure

Failure Data,

I suppose groupSelect gives me witch RAM group  or RGS and RDS values, but I don't know witch.

DataSelect I don't know what is.

address is the offset from the base address of the RAM group, but as I don't know witch group is, I don't know witch device has failure for certain.

If the groupSelect is the Ram Group, I would be DCAN2 and MIBSPI3.

And data is the failure data.