I am using evaluation board which is having LM4F232H5QC controller.
while I am commenting some part of code and try to debug using code-red debugger it is working fine.
But when i am not commenting that code, it is allowing me to debug for 2-3 times. After that it is giving error as following
"15: Target error from commit Flash write"
and
"target error from read memory " after the above one and i have to stop it then......
plz give me the solution and know me what can be the problem.
I searched another websites. They are telling that "power may not connected to the device properly" or "device is not getting proper value of current". I have tested that but i don't think that it can be the issue.......power supply is given properly.