Other Parts Discussed in Thread: HALCOGEN
Hi
I have a project where I have to use timer to generate for two purposes
1.generate timer output frequancy of 500Hz for half sec and than nothing
2.generate timer output frequancy of 600Hz for half time and than 900Hz
3.count input pulses when sig en is '1' and if en='0' not count the input pulses
there is way to implimment the alghorithem without using HET IDE only with halcogen (I have to make as fast as I can its urgent) only with halcogen
Thanks a lot Yehonatan