Hi,
does anyone know if the Fapi_HardwareCalculateEcc function works on the TMS470M? I am using the API 1.06, which is the latest off the website.
I have run the function on 16 bytes, 4 32bit words, and the resultant ECC words returned appear to be the same, regardless of the data that I have programmed into the memory.
If the ecc function does not support the TMS470M processor, where can I find the algorithm so that I can create my own function to calculate the ECC?
thanks for the help, I am away for 2 weeks, so if I won't reply back until I return.
regards,
Phil