Hello,
Apologies if this is in the wrong place, I could not add a new post to the development tools forum because there was no relevant subgroup that allowed me to post.
I have an EKK-LM4F232 eval board, and have been using it to develop my application for a project board that has the 64 pin version of this part. I have been able to program flash on the eval board microncontroller, but now need to program the device on my project board.
I have searched for days on the ti.com knowledge base, forums, application notes and user manuals for the eval board. I cannot find anything that describes if and how the eval board can be used to program my project board device.
On the eval board user manual schematics, I can see a 10 pin connector called external debug, which I assume can be used for this purpose, but nowhere can I find any description of how to do this or configure either Keil or the LMFLASH utility.
Can someone tell me if this board can be used for this purpose, and if so, point me to a document that describes the process.
Thank you
Robert Morrison