Other Parts Discussed in Thread: HALCOGEN
I want to measure a signal of about 1 MHz. using the TMS470 MF06607
I have tried using the PCNT algorithm on the HET, but unfortunately the algorithm has given results that are inconsistent around this frequency, sometimes varying from the true periods by 50% or more.
So I have been looking into using ECNT to count external pulses. I could then interrupt the ECNT counting with some kind of Real Time Counter.
Is the best (or only) way to do this involve the RTI peripheral? (the RTI peripheral would wait for x cycles before interrupting the HET)
Thanks in Advance,
Charlie