I have a question regarding the main oscillator. We are planning to use a 16MHz crystal to generate TI clock, which is the same frequency as the crystal on the TI Eval board. However, we would like the ability to spread (using SSCG) this clock (we have an external part for doing this). One idea is to have a schematic/layout that supports either having the crystal or the external clock generator chip connect to the TI part via resistor pops/de-pops. If we used the external clock generator, we may want to spread the clock as much as 3%.
What are your thoughts regarding both the clock frequency and spread range as well as having a a non-standard PCB layout with regards to the crystal? I know there is a TI Stellaris app note with suggestions about the layout of the crystal circuit. How much can we safely deviate from this. Is it just a general suggestion, or is the Stellaris part particularly sensitive in this regard.