Other Parts Discussed in Thread: HALCOGEN
Hi,
How to use Output Multiplexing and Control in TMS570LS30336 Micro for configuring GIOA[7] as NHET2[16].
Please help.
Regards,
Priya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: HALCOGEN
Hi,
How to use Output Multiplexing and Control in TMS570LS30336 Micro for configuring GIOA[7] as NHET2[16].
Please help.
Regards,
Priya
Hello Priya,
We have this same question in another thread located at the following link:
Configuration of MUX register in TMS570LS
This question is currently open as I am trying to get clarification of the part number being used since the mux configurations are part number dependent and the part number you have provided cannot be identified. However, as a general rule, the mux configuration code generation is available in Halcogen. With this tool, you can select the alternate pin functions and output the configuration code. However, as I mentioned, the part number you have provided is not in the list so I am curious if there is a misunderstanding about the part number. Can you tell me the literature number of the datasheet you are using so I can investigate further?
Hello Priya,
I have received clarification from the device owner that the TMS570LS30336 was an early part number for the device and it was updated to TMS570LS3137 prior to release to market.
To aid in configuring the IOMUX for the TMS570LS30336 part you are using, please use the HalCoGen tool that is available at the link below:
http://www.ti.com/tool/halcogen
When using this tool, select the TMS570LS3137 device for the project and then configure the IOMUX per your application needs.
Hello Priya,
If this post was able to answer your question, please click on the verify button ao that the thread can be idicated as resolved for others that utilize the forum for support. In the meantime, I will close the thread. If there are any additional questions or need for help, please start a new thread.