This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Samtech connector on LM4F232 eval kit

I was told that the Samtech connector TFM-110-02-S-D-K-A is discontinued. Is there another vendor who makes the compatible connector?

  • Believe there is a jumble in your part number: "-S denotes single row; -D denotes double row."   Doubt presence of both is legal - may confound system -  thus register as, "discontinued."

  • As far as I know the part is still in production. Try building a part on Samtec's website with the following parameters:

    Series: TFM
    Pin Center: -1

    Positions: 10 
    Lead Style: -02
    Plating: -S (Selective Gold)
    Row: -D (Double Row)
    Alignment: -A (Alignment Pin)

    Pick and Place Pad: -K (Polymide Film)

    These choices generate TFM-110-02-S-D-A-K.

    Obviously the pick and place pad is optional.

    -David