Hi there,
Can I connect both nPORRST pin and nRST pin together and drive them using a single MAX811 chip (Power on/Manual Reset)?
Thanks,
Brent Shen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
Can I connect both nPORRST pin and nRST pin together and drive them using a single MAX811 chip (Power on/Manual Reset)?
Thanks,
Brent Shen
Brent
This is not recommended. As you realized from reading the datasheet our nRST is a bidirectional pin. If you assert the PORRST, then device drives nRST low immediately. Now if you release NPORRST the device continues to drive nRST low for another 8 VCLKs. At this point you will see contention between a high being driven by outside and a low from the device. You can't use a pull-up on NPORRST (while shorting with NRST) either because then the device will always win and you will never be able to come out of reset.
Regards
Abhishek