Greetings:
Have past squawked - long/hard - to no avail (seemingly). Despite being semi-literate and motivated - I can never/ever "quickly/easily" locate - the Stellaris "MCU-Class" cataloged listing. If this exists - its "promotion" leaves something to be desired.
As StellarisWare regularly expands in capability - and not all new functions succeed across all MCU classes - the need for such "Class Catalog" boils bit closer to the surface... Avoidance may no longer be best/only, "resolution." (ya think?) Here - this reporter's "one-stop" means to more efficiently convey the intrusion of "Class" - into/upon StellarisWare...
Stellaris MCU....................Class........................StellarisWare - Limitations/Exclusions (if any)
LM3S101............................Sandstorm...............GPIOPinConfigure(), (surely more - this just as example)
LM3S811............................Sandstorm...............GPIOPinConfigure(), (as above)
LM3S1627..........................DustDevil.................GPIOPinConfigure(), and others
LM4F232............................Blizzard....................No Exclusions (hurray)
Chart shown above - of course size-limited - but clearly representative of, "best practice" method to easily/quickly "decode MCU-Class" mystery. Current method - force each/every Stellaris User to reinvent the wheel - searching God knows where - somehow seems tad uncaring, inefficent - poorly crafted! Vastness of number - superior access to data - and in-depth training argues very much in favor of forum Staff performing this classification. Curious that this wound remains - so long untreated...
Long ago we were taught that Sales are much aided via: Comfort and Convenience. Neither are prominent in this long-percolating, unwanted - "Class Intrusion" upon the otherwise superb, StellarisWare.