Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Greetings,
I am using the tms570 HDK. I have configured the LIN module in sci mode. The baudrate is set to 9600. I have a usb to serial converter that I am trying to use to send data to the board. When I measure the output of the usb-to-serial converter before it is connected to the board, I can see all the uart messages being sent out. However, once I connect the board to the converter and try to see the messages, I find that the line (TX from usb-to-serial, LINRX on board) seems to be pulled high the entire time. Any ideas?
Thanks alot.