I use HET IDE 3.2. When editing het of the file in the project (for example instruction replacement one on another), and at the subsequent compilation doesn't occur.hnc file replacement. Therefore at simulator start in a "full dissasembly" window the aged code which was before editing is observed. How to avoid this behavior? The conditional example of the project I apply. I make comments in turn on L01 and L02 labels.