Other Parts Discussed in Thread: HALCOGEN
Hi,
I use the The HalCoGen 2.11 and 3.00.01 and now the 3.01.01. The update from HalCoGen 3.00.01 to 3.01.01 have a lot Problemes.
The Notivication.c is not good, the "while(1);" is a great Problem, when I change this in "return;" and "generated code" new the write the same "while(1);" in the code, this is poor.
Next problem is "_memoryInit_" is defined in sys_memory.asm without parameters, when I compile the project is the "_memoryInit_" the double defined, in the sys_memory module and in the sys_selfttest module.
Then I create the GCM become I the windows with VCLK1 and VCLK2 is the zero! and the VCLK1 Config and VCLK2 Config can't change? ups? Look in HalCoGen 3.00.01 is the VCLK's adjustment correct.
Can Your fixed this Problem? please betimes
Your HalCoGen is amazing, just important function lost such as those DMA....
Best Regards
Rolf Timm