Other Parts Discussed in Thread: TMS320F28335
I try to connect our new blackhawk xds560v2 STM emulator to TI's TMS570 development board. I connected to this board before using the on-board xds100 emulator. With the new configuration however, I get the following error message:
Error connecting to the target: (Error -234 @ 0x0) The instruction scan-path cannot circulate bits, it may be broken. An attempt to scan the JTAG instruction registers has failed. The target's JTAG instruction path appears to be broken with a stuck-at-ones or stuck-at-zero fault. (Emulation package 5.0.791.0)
With the emulator, some config and diagnostic tools are supplied. If I try a JTAG path scan with the "BH560v2 config utility", it always works the first time after powercycling the development board. All the times after that, the same test will fail. I browsed through several threads here on the forum, and I already tried following suggestions:
- update the emulator firmware
- update the emulator drivers (through code composer)
- reduce the JTAG clock (down to 0.5 MHz)
- set the acces port designator to 0x02000100
None of this seems to work. I am a bit out of ideas now, and I would like to ask if any of you would have some further suggestions?
thanks already,
Bert