This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Implementing EtherCAT on Hercules platform

Other Parts Discussed in Thread: RM48L952

Hi, 

We are focused on implementing Ethercat protocol on Hercules platform powered board which will be connected in mixed (star and ring) topology. According to my limited knowledge, Ethercat protocol could be implemented by using 1 ethernet port if it is used only with star topology, 2 ethernet ports if it is used whether in star or ring topology, 3 ethernet ports if it is used in mixed (star and/or ring) topology. If I'm not wrong, then we need 3 ethernet ports but RM48L952 has only one ethernet port. So, there is a problem.

We are considering using Hercules with http://www.beckhoff.com/english.asp?ethercat/et1100_et1200.htm or Sitara platform instead of Hercules platform. Safety is the most important feature for us.

Is there any suggestions?

Thanks.