Hi,
How can i watch the oscilloscope display in pc for stellaris LM4f232/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You almost answer your own question! As you state - the Stellaris MCU systematically "reads/logs" the pertinent data - the mechanics reveal w/in the provided source code. Thus - to exploit a larger screen - would not you send that data to the PC - as one additional step w/in the existing StellarisWare program?
You'd have to decide/choose most suitable transfer medium and then develop your own PC program from scratch - or use one of many existing data log/display programs - or feed the data into a spreadsheet program for even deeper statistical analysis and display...
Many ways to bite this apple...
I looked at the comments at the top of the qs-logger program...
It said this...
//! A companion Windows application, logger, can be found in the
//! StellarisWare/tools/bin directory. When the data logger's STORAGE option
//! is set to "HOST PC" and the board is connected to a PC via the USB OTG
//! connection, captured data will be transfered back to the PC using the
//! virtual serial port that the EK board offers. When the logger application
//! is run, it will search for the first connected EK-LM4F232 board and display
//! any sample data received. The application also offers the option to log
//! the data to a file on the PC.
//
Just read all the comments at the top of the program. It's the rtfi system.