Hello.
My problem is that the termination of the debug session led to the crash of the memory, then computer was rebooted. After that, on the development board TMS570 LS3137 dimmed power-LEDs and power to the board is not supplied. P1 connector on the voltage 5.2 V. I suspect that the problem is in the converter from 5V to 12V.
Please answer me how to solve this problem.
Thanks.