This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with power on TMS570 LS3137

Hello.

My problem is that the termination of the debug session led to the crash of the memory, then computer was rebooted. After that, on the development board TMS570 LS3137 dimmed power-LEDs and power to the board is not supplied. P1 connector on the voltage 5.2 V. I suspect that the problem is in the converter from 5V to 12V. 

Please answer me how to solve this problem.

Thanks.