Other Parts Discussed in Thread: LMFLASHPROGRAMMER, SYSBIOS
I received board with data logger app preinstalled and it worked great. I then tested and loaded a few example programs to get familiar with process. Everything worked well. I now want to reload the Data logger app back into the board the the Keil uVision4 app reports after compiling it is 39K size and to big to load. I erased all programs from board. There is only 32k of flash memory on the board.How can I reduce the size of the data logger program or change what memory I store it in Like the 256K of SD memory on Chip?