Other Parts Discussed in Thread: SYSBIOS
I'd like to get a linux kernel running on the LM4F. I know it doesn't have a mmu, but I know there are some distros out there that support it. Which ones would that be?
Will uClinux work?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSBIOS
I'd like to get a linux kernel running on the LM4F. I know it doesn't have a mmu, but I know there are some distros out there that support it. Which ones would that be?
Will uClinux work?
Thanks
Michael:
Maybe. The LM4F232 board is a little light on RAM. IMHO anywway.
The Stellaris LM4F232H5QD is an ARM® Cortex™-M4F-based microcontroller with 256-KB Flash
memory, 32-KB SRAM, 80-MHz operation, USB Host/Device/OTG, Hibernation module, and a
wide range of other peripherals. See the LM4F232H5QD microcontroller data sheet (order number
DS-LM4F232H5QD) for complete device details.
Comment from someone else trying this...
I could not find an open source uClinux implementation for Kinetis K70, but emCraft has a Linux Board Support Package (BSP) for the Freescale TWR-K70F120M-KIT hardware platform available for 99 USD.
Dave Robinson said:LM4F232 board is a little light on RAM. IMHO anywway.
Mon ami - not a whole lot of humble from you/I.
Re: "little light on RAM"; is that like saying your HMS Titanic is now, "little light" on flotation?
As you report - extending such memory-shrunk MCUs appears far from their, (and desired Apps) "sweet spot."
CB1:
I did not want to say "impossible" -- just to suggest better use of time. ;-)
You have discovered my weakness -- the shame of it all. I do not have a hair shirt -- so I compiled a C2000 app before lunch as penance. Did I mention that I hate static linkers? No? Well I do...
Give me an M3/M4 CORTEX any old day -- Just not for Linux.
Yes -- Titanic designers/engineers skipped stress analysis section of Iron Plate and Rivets Class at UEA -- it was "somewhat light on the flotation specs". Let this be a caution to all designers to eschew the use of under-rated parts.Proper research is required to maintain discipline.
'Nuff said! (Thanks for the chuckle! -- keep them coming!)