This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2 TMS570 Boards Connected in 1 PC

Hi All,

I got 2  TMDX570LS20SUSB  boards connected in one PC. I wanted this two boards communicate with each other using CAN Communication, so I created  2 projects in CCS4 - (1) CANTransmit and (2) CANReceive.

I wanted the CANTransmit application to run in one board and then the CANReceive application  to run in the other board.

Is it possible to launch 2 Debug Sessions in CCS4 at the same time so I can verify the transmission/reception of data through CAN? If yes, how do I set it up?

Thanks.

Regards,

Dennis