My guess someone screwed up in the Bom when they designed the Hibernate battery holder. I notice the part number for that holder is also wrong from Digi Key. The documentation says it takes a CR2032 3v Lithium. That battery is 2cm in diameter. The holder will only take about an 11mm diameter battery. Has anyone found a battery that will fit the holder. I don't want to add a 2032 holder because the board has little room for it. I prefer finding a battery that will fit the existing holder. Surely others have noted this. Thanks for any help on this.