Hello,
I'm in the process of designing a LM4F board and am wondering if the firmware for the LM3S3601 ICDI from the LM4F232 Eval board is available publicly or not?
I realize I can just add a standard 20 pin jtag header and then use something like the LM3S811 eval kit (I'm using Code Composure Studio on the software side) but given I'm developing a custom board anyway it seems like just adding on board debug support (along with USB power) would keep things simpler. Longer term (this is meant to be a development kit product) having customers not have to get something else in addition for debug seems like a good thing...
Or, for this level of support, am I just better off using the FTDI chip? As far as Code composer studio features would this be equivalent?
Thanks for your help!
Shannon