This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48 HDK input GIOB[2] problem always high

Hi,

I have problems with using GIO[2] as in input pin on my HDK  with RM48 L950AZWIT.

Bit is always high.  My test procedure: start-up, nothing connected, and bit is high.

I tried set GIOB[1] as an output and connect to GIO[2] and no success. If i connect GIO[1] as output and GIO[0] as input. it works fine.

I use F2 pin for now, but later i will like to use V10. I read that if i wanna use V10, i have to write 1 to  PINMMR29[16] .

Is that true?