Hi all,
Does anybody know where I can acquire the BSDL file for the TMS570LS3137?
EDIT: It's not on the wiki.
Thanks in advance,
Matt.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Does anybody know where I can acquire the BSDL file for the TMS570LS3137?
EDIT: It's not on the wiki.
Thanks in advance,
Matt.
Matt,
I am assigning your query to dave who is responsible for the BSDL . He will work with you on this.
Hercules forum support
The TMS570LS31xx BSDL files are now available on their product page under Tools and Software.
Here is a link the TMS570LS3137PGE.
Thank you.
Hi Dave
I can only find BSDL files for PGE Packed.
Can you provide a model for ZWT packed. (TMS570LS3137ZWT)
Thanks in advance
Benny.
Benny,
The BSDL models for the TMS570LS31xx devices are available on their product page under Tools and Software.
Here is a direct link to the TMS570LS3137ZWT BSDL file.
Thank you,
Forum Support
Hi
I have also look at TMS570LS31XX but it i expect a different pin mapping than P1 to P286
I would expect somthing like A6 or M2
Benny.
Benny,
That is a great point, the existing numbering system will not affect the usefulness of these files but we will update the files to match the numbering system in the datasheet.
Thank you for your feedback,
Forum Support
Hi
When I'm using the BSDL files in TestWay, it doesn't look right.
if the existing numbering system doesn't affect the usefulness of these files, why is there?
I would very much like to try with a file with the correct pin numbering.
When could that be possible?
Thanks and a happy new year
/Benny
Hi
I need a BSDL file for TMS570LS3137ZWT with correct pin mapping.
Can you provide this for me?
Thanks.
/Benny
Benny,
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/312/8666.TMS570LS31xxZWT.bsdl
Here is the updated BSDL file for the TMS570LS31xxZWT with letter/number pin names per the datasheet.
I will also submit these to be updated on the device webpages for future downloads.
Thank you,
Forum Support
Hello Benny,
Did Dave get you all the information you needed to resolve your issue with the pin names? If so, please verify his last post so that the thread may be closed.
Hi
no, i'm completely satisfied.
I was hoping to find a BSDL file with correct pin mapping an all pins.
it seems the linkage pins has not been changed to match ZWT packed.
I need a correct mapping of all pin, to be able to use it in TestWay.
I hope you can provide this to me
thanks.
Benny
Benny,
I apologize that this BSDL file did not work as you expected, I see that some of the linkage pins still had the old numbering scheme.
I've updated the file to match the ZWT exactly, powers and grounds are bit vectors and no pins have the old numbering scheme.
I hope this is what you are looking for.
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/312/7701.TMS570LS31xxZWT_5F00_v1p4.bsdl
Forum Support