Other Parts Discussed in Thread: TMS570LS3137
Hi,
Is it possible to interface synchronous SRAM (CY7C1383D) to TMS570LS3137 using EMIF ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS570LS3137
Hi,
Is it possible to interface synchronous SRAM (CY7C1383D) to TMS570LS3137 using EMIF ?
Dalin,
I checked the CY7C1383D spec. It is not compatible to TMS570LS3137 EMIF.
Thanks and regards,
Zhaohong
Dalin,
Here are some example external memory devices that are compatible with TMs570LS3137 EMIF.
SDRAM: MT48LC8M16 and asynchronous RAM: IDT71V416.
The following thread has the information about the how endiannes affects the use of external flash.
http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/218806.aspx
Please let me know if the above solves your problem.
Thanks and regards,
Zhaohong
Hi,
It is not clear to me why the CY7C1383D is not compatible with the TMS570 family. Can you elaborate? Is the CY7C1441KV33 compatible? www.cypress.com/.../download
Thanks,
DJ
DJ,
TMS570 EMIF only supports two types of memory interface: asynchronous and SDRAM. You can compare the access waveforms of the supported interface in the TMS570 TRM with the cypress memory.
Thanks and regards,
Zhaohong
Dear Zhaohong,
Is it possible to interface Synchronous DPRAM to TMS570LS3137 through SDRAM Interface ?. The part number of Sync DPRAM is CY7C09099V-12AXC. I have attached the schematic of we interfaced please have a look at it and reply if it is correct or not.0246.TMS_FPGA_DPRAM.pdf