Other Parts Discussed in Thread: TMS570LS3137, TMS570LS20216
Hi there,
I have some questions regarding nPORRST and nRST pins of TMS570.
1) Do I need both pins reset when TMS570 is powered on? Or nPORRST alone is enough?
2) What if two active low pulses (~ 200 ms) are applied at both nPORRST and nRST at the same time? (Although it's a weird question but please answer it for me)
The reason why I ask the two questions above is because right now I am using two MAX811 (pwr-on reset) chips which are connected to nPORRST and nRST individually. The problem I have is that TMS570 occasionally resets correctly and sometimes it doesn't.
Thank you so much.
Regards,
Brent Shen