Other Parts Discussed in Thread: RM48L952, HALCOGEN, TMS570LS1227, RM42L432, RM46L852, RM48L530, RM48L540, RM48L730, RM48L740, RM48L940, RM48L950
When trying to start a debug session from CCS 5.2.1.00018 on a RM48L952 HDK development kit, the following error shows up:
CortexR4: Flash Programmer: Missing Erase Settings.
CortexR4: Flash Programmer: Error erasing Flash memory.
CortexR4: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x5308
CortexR4: GEL: File: D:\workspace_TI\TMScontroldevice\Debug\TMScontroldevice.out: Load failed.
NowFlash and the demos can successfully program the device, although nowFlash has a tendency to time out from time to time. If I flash the HALcoGEN generated basis without any modifications with nowFlash, the red error led turns on after resetting the device.
At first I thought it was a CCS error, so I made a thread in the CCS forum first, but it seems the default troubleshooting steps didn't help.
Any feedback is greatly appreciated!