This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Erroneous "Feature" on the LM4F2xx Series: External Peripheral Interface (8/16/32-bit dedicated parallel bus)

Hello,

Under the "Features" heading of a few of the LM4F series product pages it states that one of the of features of the device is that it has a 8/16/32-bit dedicated parallel bus.  However, I can not find any reference to such bus in the datasheet.   One example of this is found on the the LM4F120 product page: http://www.ti.com/product/lm4f120h5qr.  Click on the "Show More" button under "Features".  The same can also be seen in the following:

My guess is that this is a copy/paste error because the External Peripheral Interface (EPI) exists in the LM3S datasheet (http://www.ti.com/product/lm3s2d93).  
Can you someone confirm the absence of this peripheral on the LM4F series processors?
Thanks