Other Parts Discussed in Thread: HALCOGEN
Hello.
I get a new HDK from TI.
And I made a project using HALCOGEN and CCSv5. (JTAG is XDS100v2 USB)
When I debuging this project, I cannot connect the HDK.
Error message is " Error connecting to the target: (Error -183 @ 0x0) The controller has detected a cable break far-from itself. The user must connect the cable/pod to the target. (Emulation package 5.0.747.0)"
So, I opened the debug configuration file xxxxxxx.ccxml.
and execute "Test Connection" . Result is
"
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\ahns79\AppData\Local\.TI\2620625255\ 0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusb.dll'. The library build date was 'May 30 2012'. The library build time was '22:52:27'. The library package version is '5.0.747.0'. The library component version is '35.34.40.0'. The controller does not use a programmable FPGA. The controller has a version number of '4' (0x00000004). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal. The controller is the FTDI FT2232 with USB interface. The link from controller to target is direct (without cable). The software is configured for FTDI FT2232 features. The controller cannot monitor the value on the EMU[0] pin. The controller cannot monitor the value on the EMU[1] pin. The controller cannot control the timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '0' (0x0000).
-----[The log-file for the JTAG TCLK output generated from the PLL]----------
There is no hardware for programming the JTAG TCLK frequency.
-----[Measure the source and frequency of the final JTAG TCLKR input]--------
There is no hardware for measuring the JTAG TCLK frequency.
-----[Perform the standard path-length test on the JTAG IR and DR]-----------
This path-length test uses blocks of 512 32-bit words.
The JTAG IR instruction path-length was not recorded.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 512 32-bit words. This test will be applied just once.
Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-183' (0xffffff49). The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.
The explanation is: The controller has detected a cable break far-from itself. The user must connect the cable/pod to the target.
[End]"
What is the problem? I just get the new HDK.
What is meaning of this message.
"There is no hardware for programming the JTAG TCLK frequency."
"There is no hardware for measuring the JTAG TCLK frequency."
Please Help me!