This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS470R1A384 Questions




1. The datasheet states that there is a digital watchdog timer (DWD) but there is no additional mention of that timer in the SPNU189 documentation.  Is this timer a part of this micro and if so where can I find documentation on it?

2. We are grounding the AWD pin with a 10kohm resistor because we are not using the AWD function.  Is a 10kohm resistor adequate to ensure the AWD pin does not trigger a reset?

3. Is there any reset (AWD or DWD) related errata that we should be aware of on this device?