This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 ADC Module

Hi there,

Under the circumstance that both VCC and VCCIO pins of TMS570 are 3.3V, can I set the VCCAD and ADREFHI pins to 2.5V so that the input range of the ADC module is 0 ~ 2.5V? Is there some anti-alias feature built into the ADC module of TMS570? Thank you.

Regards,

Brent Shen