This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WDRST Bit and EXTRST Bit are set together in SYSESR Register



Hello Support,

When there is a Digital Windowed Watchdog Reset, I see within SYSESR Register,

WDRST as well as EXTRST bits are SET simultaneously.

I thought only WDRST bit will be set during Digital Windowed Watchdog Reset.

Please clarify in case there is a Power Supply issue in the HDK board.

Thank you.

Regards

Pashan

 

  • Pashan,

    When a Digital Windowed Watchdog Reset occurs, the device will set the corresponding flag in SYSESR.
    This reset condition is also driving the nRST pin low. This pin is an I/O, so the system module will catch this reset as external.

    At then end, both flag are set in SYSESR.