Hello,
I'm developing on a TMDX570LS20SUSB kit with XDS100 and have a problem:
When I want to flash, I get the following errors:
in nowFlash v3.42: Error 199 - Unable to connect to target on port address 0x000
in code Composer Studio v4.2.3:
Error connecting to the target:
(Error -151 @ 0x0)
This utility failed to open the adapter for a custom emulator.
The adapter returned an error.
(Release 5.0.333.0)
I've read this thread: http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/130226.aspx and tried the hint of Mr. Weng in the verified answer (I used the Reset-button), but it doesn't work. (By the way: when I click the Reset-Button, no blue LEDs are blinking any more)
I also reinstalled the driver and the CCS, but it doesn't work, too.
In the microsoft device manager, the kit is listed under the USB-Controller as USB Serial Converter A and B and one USB-Verbundgerät - all three devices without errors.
The crazy thing about it: it worked a few days ago! In the meantime, I developed with the "HET Simulator" - but that doesn't matter, does it?
Mr. Weng also wrote something about the C5 on the back of the board - I found it, but am I allowed to short it? Can I destroy the board by shorting the C5?
I hope, you can help me.
Thank you in advance.
Kind regards,
Lena