This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help with locked LM4F232

Hi everyone,

I've accidentally changed a pin (PC0) belonging to the JTAG interface to be used as a GPIO on my evaluation kit (http://www.ti.com/tool/ek-lm4f232) with a LX4F232H5QD chip.
Now I'm locked out. I tried to unlock it by using "Debug Port Unlock" in the LM Flash Programmer utility.
For this procedure I connected pin 10 of the JTAG connector to ground.
In the LM Flash Programmer I've selected "Fury, DustDevil, and Blizzard Classes".

Nothing helps, all I get is: "**ERROR**: Failed to unlock connected device!"

I also tried using a XDS100v2 instead of the onboard ICDI interface.

Can anybody help?

Thank you,
Stefan

  • Cross-post!   Note - original post stated Sandstorm class device - has subsequently been changed...  Poster at least is consistent - having locked himself now out of 2 Stellaris.

    LX4 devices are, "Blizzard" - should select that using LMI Flash Programmer and follow exact Unlock Procedure...

    http://e2e.ti.com/support/microcontrollers/stellaris_arm_cortex-m3_microcontroller/f/471/t/225049.aspx

    Response w/in reference...

  • Sounds like a good idea to halt the MCU, unfortunately I don't think it will help in my case as I do the configuration of GPIOs right at the beginning.

    Any other ideas?

  • Still unclear if yours is an LX4F or LM3S-Sandstorm.  Those early class (Sandstorm) parts - as I understand - did not include any facility to, "unlock."  If instead - as your Subject now states - yours is LX4F - the normal Utility "unlock" w/in the flash programmer should quickly restore.

    Theory (and we/others have done this w/success) is to force the Sandstorm MCU to "hang" prior to reaching the errant JTAG instruction.  If that instruction is the earliest - you may well have to remove/replace that MCU. 

    Prevention trumps cure dept: "written notice - re: Port_C and Sandstorm - is prominent @ all our workstations..."  

  • It's an LX4F. I just wrote to customer service about the problem. If they're able to help I'll post the solution here.

  • Stefan Ineichen said:
    I'll post the solution here.

    Such is always appreciated - will likely return you faster and more considered response on future posts.

    Blizzard class does appear on newer LMI Flash Programmer Tool.  Suggest that you upgrade to newest version - select Blizzard and attempt unlock procedure.  Suppose that if yours is lunchpad or eval - possibly "unlock" not fully implemented - but have yet to encounter dreaded, "lock-out" on LX4F family...

    Do post end results and good luck...

  • Thanks for the suggestion.
    The blizzard classes already appeared in the LM Flash Programmer version I had installed.
    I've updated to the newest version regardless and the problem is still the same.
    Hopefully the people from customer support answer quick...